This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6747A: RTCLOCK bit (RTCLOCK feature)

Part Number: MSP430F6747A


Hello Support member

There is the following description in SLAA666A.(In P3)

3 Addition of RTCLOCK Feature
In the MSP430F67xxA devices, a RTCLOCK feature has been added to reduce the amount of reconfigurations that are necessary after a reset.

SLAU208Q has the following description.(Fig 24-7)
(1) This bit is implemented in only the F677xA, F673xA, and F672xA devices. For other devices, this bit is reserved and always reads as 0.

Q1.
MSP430F6747A does not have a RTCLOCK bit (RTCLOCK feature).
Is this understanding correct?

Best Regards,

**Attention** This is a public forum