Hi experts,
Let me check the setting of the EUSCI register (UCBRSx) in the following system.
SMCLK = 16.384MHz/4 = 4.096MHz
N=4.096MHz/38400bps = 106.6666...
In the above case, which is correct?
- Rounding up the decimal point: UCBRSx=D6h
- Rounding down the decimal point: UCBRSx=B6h
By the way, in the simulator below, "UCBRSx=B6h" was used.
MSP430 USCI/EUSCI UART Baud Rate Calculation
:software-dl.ti.com/.../index.html
Best regards,
O.H