The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: LCD problems on EVM430-FR6043 with the TIDM-02005 reference design

Part Number: EVM430-FR6043
Other Parts Discussed in Thread: TIDM-02005

Hello, I have the EVM430-FR6043 board and I am experimenting with the reference design TIDM-02005. However, I am having an issue with the LCD. After I flash the board with the code, I click the "Select" button and the LCD displays the data (Volume, DTOF, AVG DTOF, etc.). When I click the "Reset" button and then on the "Select" button the LCD will no longer turn on, the same thing happens if I disconnect the board from the USB (which turns it off because I am using USB to power it). In the USS Design Center I can see that the board is taking measurements so it is running the code, except the LCD does not show anything.

Summary: I flash the board with the code, press the "Select" button and the LCD turns on. Then if I disconnect it and reconnect it from power or click the "Reset" button the LCD no longer turns on when I click the "Select" button. However, in the USS Design Center I can see that it is still making measurements so I can assume that it is still running the code.

**Attention** This is a public forum