For XT2. What is the range of crystal ESR that is recommended?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Lauren,
We do not specify ESR values for requirements of XT2. However, we do specify Oscillation Allowance which is effectively the max ESR allowed with a safety factor test result of 5. For more information about the relationship of ESR and OA, see section 2.2 ESR values of the following app note: MSP430 32-kHz Crystal Oscillators
Note: the app note linked is centered around LFXTALs; however, the same principles apply for HFXTALs.
**Attention** This is a public forum