Hi
I made a PCB for prototype with 3 LC sensors, but I need the reversed order of scanning these sensors. There are two options, I change PCB again or reverse order how the firmware handles them. The reason that I want to reverse order is that interrupt is triggered on positive rotations and when my reading device has normal rotations in reverse direction, then I have to read counters "manually" because these interrupts when whole 1 rotation is done don't occur at all. So I've changed PSM in which I have swapped left with right states everywhere, also I changed TSM table, and the first channel excited is number 1 instead of 0, but still it triggers interrupts in the wrong direction. Does anyone knows what else to change?