This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2353: No I2C Interrupts

Part Number: MSP430FR2353
Other Parts Discussed in Thread: MSP430FR2355, HDC2080, HDC2022,

I am trying to port the sample code in /msp430fr2355_demo_with_hdc2080/main.c to our hardware (FR2353, HDC2022). I'm using USCI_B1.

The I2C peripheral is not generating an interrupt (never hits the breakpoint I set on the first statement in the ISR).

First of all, am I using the correct keyword in the statement below:

#pragma vector = USCI_B1_VECTOR

How about this?

#pragma vector = EUSCI_B1_VECTOR

Do both point to the same interrupt vector?  Both Build with no errors.

Here are some of my code snippets that were modified to match my hardware.

void initGPIO()
{

......... skipped lines

// I2C pins (P4.7 is SCL, P4.6 is SDA)
P4SEL0 |= BIT6 | BIT7;
P4SEL1 &= ~(BIT6 | BIT7);

.......skipped lines

}

void initI2C()
{
UCB1CTLW0 = UCSWRST; // Enable SW reset
UCB1CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C master mode, SMCLK
UCB1BRW = 160; // fSCL = SMCLK/160 = ~100kHz
UCB1I2CSA = SLAVE_ADDR; // Slave Address
UCB1CTLW0 &= ~UCSWRST; // Clear SW reset, resume operation
UCB1IE |= UCNACKIE;
}

//******************************************************************************
// I2C Interrupt ***************************************************************
//******************************************************************************

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_B1_VECTOR))) USCI_B1_ISR (void)
#else
#error Compiler not supported!
#endif
{
//Must read from UCB1RXBUF
uint8_t rx_val = 0;
switch(__even_in_range(UCB1IV, USCI_I2C_UCBIT9IFG))       <<<<<<<<<<<Breakpoint set here.....
{

.......

......

}





I2C_Mode I2C_Master_WriteReg(uint8_t dev_addr, uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
/* Initialize state machine */
MasterMode = TX_REG_ADDRESS_MODE;
TransmitRegAddr = reg_addr;

//Copy register data to TransmitBuffer
CopyArray(reg_data, TransmitBuffer, count);

TXByteCtr = count;
RXByteCtr = 0;
ReceiveIndex = 0;
TransmitIndex = 0;

/* Initialize slave address and interrupts */
UCB1I2CSA = dev_addr;
UCB1IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts
UCB1IE &= ~UCRXIE; // Disable RX interrupt
UCB1IE |= UCTXIE; // Enable TX interrupt

UCB1CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts   <<<<<<<<<<<< HANGS HERE...............

return MasterMode;
}

When I run the program, it hangs on the line:

__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts

The breakpoint is not hit.

This is the first attempt to use I2C to talk to the HDC2022).

**Attention** This is a public forum