Hi All,
I am using MSP430FR2475, my lora code working if both device and gateway with same controller. but cross controller like msp430 and esp32 notworking. i am using sx1262 lora module.
please suggest any settings needed.
Thanks in Advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I am using MSP430FR2475, my lora code working if both device and gateway with same controller. but cross controller like msp430 and esp32 notworking. i am using sx1262 lora module.
please suggest any settings needed.
Thanks in Advance
Hi Vinod,
The connection between MSP430 and SX1262 should be SPI interface, right? Does not work mean something is error with the SPI or others?
Thanks!
Best Regards
johnson
Hi Johnson,
Yes, LoRa is SPI communication.
The LoRa is Communicating between two MSP Devices or Two ESP32 Devices, If Msp Broadcast Data, I am unable to get in the ESP device
Thanks,
Vinod
Hi Vinod,
It seems that not MCU issue, maybe you can capture some wave using logic analysis.
Thanks!
Best Regards
Johnson
**Attention** This is a public forum