This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F249-EP: MSP430F249MPMEP

Other Parts Discussed in Thread: MSP430F249

Hi,

I am developing a card with msp430f249mpmep micro controller.

I use with UART protocol at a baud rate of 430.2Kbps and with internal ADC.

The micro controller will operate in a wide temperature range: -55 deg to 105 deg.

Is it possible to use the internal clock 16Mhz? or I have to connect an external clock at frequency 16MHz?

If I need to connect an external clock, you may recommend For an oscillator component?

Regards,

Mor

**Attention** This is a public forum