Hi experts,
I want to know the maximum number of buttons for Mutual of MSP430FR2533.
When I check the link below, the maximum number of buttons for Mut of MSP430FR2533 is "24".
software-dl.ti.com/.../ch_device.html
If the captive channel is 16, then 8x8 = 64 and I think the MSP430FR2533 can use 64 buttons. Also, if I set the 64 button in the Design Center, I can pin assign without any problem.
Why is 24ch listed in the link above? Is the RAM size insufficient?
Best regards,
Sasaki