Hello All,
I have Radiation counting instrument for which we use MSP430FR5989. I have display on that instrument which displays different parameters like time, Counts, Modes, HV etc.
When this instruments counts radiation, the time which displays or shows on LCD is 2.4% faster than real life timer. So, if in real life 100 seconds that instrument will go faster and show 102.4 seconds. I tried to change in Main.c file then I found that, I could make it more faster or slower than what i have right now. How can i fix this issue to the nearest error upto +-0.5%? Your help or solution would be really appreciated.
thanks.