I want to have two possible sources to power MSP430 in my board, both 3V3. I want to connect first to DVCC pin and second to AUXVCC1. It might happen, that only one of these two sources will be available. How I should then connect any peripheral circuits that require 3V3, for example pull up resistors for I2C?
Can I connect it to VDSYS? In that case AUX will decide, which source is present and supply MCU?