Other Parts Discussed in Thread: MSP430G2553, MSPBSL, UNIFLASH
Hello,
we need to upgrade the FW on our product based on MSP430F2418 using the UART and a Windows PC as host.
You already suggets me to start from MSPBoot and start from example of MSP430G2553.
I've already created files for MSP430F2418 using MSPBootProjectCreator and I will modify the MSPBoot_F2418_UART_Dual_Img according my device but my host device is a PC, I can't use an other specific host device to upgrade our product like in the example of the bootloader_slaa600D.
If I understood correctly the MSPBoot manages the upgrade of the FW using the BSL protocol, it means is not possible to upgrade the device using a common Terminal SW (like HyperTerminal or TeraTerm) sending the application in hex ot txt format so as I get it building it with CCS, correct?
Do you have a sample app for PC that manages the upgrading of a MSP430 device with MSPBoot on board?
Do you have some guide line about how to create the image to upgrade starting from the .hex file of the application? Or a flow diagram of upgrading process ( with dual or single image) starting from .hex or .txt application file?
I really need to skip the step of using a specific host device like LaunchPad, because is very time consuming.
Best regards
Elisa