Part Number: MSP430-GCC-OPENSOURCE
Other Parts Discussed in Thread: MSP430FR5994, MSP430FR2000, MSP430FR2100, MSP430FR2110, MSP430FR2111, MSP430FR2153, MSP430FR2155, MSP430FR2310, MSP430FR2311, MSP430FR2353, MSP430FR2355, MSP430FR2422, MSP430FR2475, MSP430FR2476, MSP430FR2512, MSP430FR2522, MSP430FR2672, MSP430FR2673, MSP430FR2675, MSP430FR2676, MSP430FR5041, MSP430FR5043, MSP430FR50431, MSP430FR5720, MSP430FR5721, MSP430FR5722, MSP430FR5723, MSP430FR5724, MSP430FR5725, MSP430FR5726, MSP430FR5727, MSP430FR5728, MSP430FR5729, MSP430FR5730, MSP430FR5731, MSP430FR5732, MSP430FR5733, MSP430FR5734, MSP430FR5735, MSP430FR5736, MSP430FR5737, MSP430FR5738, MSP430FR5739, MSP430FR5962, MSP430FR5964, MSP430FR5992, MSP430FR59941, MSP430FR6005, MSP430FR6007, MSP430FR6035, MSP430FR6037, MSP430FR60371, MSP430FR6041, MSP430FR6043, MSP430FR60431, MSP430FR6045, MSP430FR6047, MSP430FR60471, RF430FRL152H, RF430FRL153H, RF430FRL154H
Good morning everyone!
bug description:
inside the msp430-gcc-support-files-1.212.zip archive, in includes/msp430fr5994.h the __MSP430_HAS_FRAM__ define is missing, but clearly is should have been set.
explanation:
in your driverlib/MSP430FR5xx_6xx/framctl.c all the functions are guarded behind a
#ifdef __MSP430_HAS_FRAM__
and MSP430FR5994 clearly qualifies as a FRAM-capable product which needs those functions from framctl.c, but inside it's header the __MSP430_HAS_FRAM__ is missing and thus during compilation the functions cannot be reached due to the #ifdef.
just had a closer look and ran these commands:
grep '__MSP430_HAS_FRAM__' include/*430fr*.h | cut -d ':' -f1 | sort -u > /tmp/have_it
ls -1 include/*430fr*.h > /tmp/all_of_them_fram_devices
diff -u /tmp/all_of_them_fram_devices /tmp/have_it | grep '^-'
it looks like there are a lot of devices that contain 430FR in their name (which would mean they got FRAM inside) and don't have that __MSP430_HAS_FRAM__ macro defined. you might want to have a look into this. list is included below if you don't have a linux machine at hand to run the commands.
possible fixes:
add __MSP430_HAS_FRAM__ define to headers that belong to devices that provide FRAM capability OR
remove the 'ifdef __MSP430_HAS_FRAM__' guard in driverlib/MSP430FR5xx_6xx/framctl.c since the entire FR5xx_6xx family is expected to have FRAM
include/msp430fr2000.h
include/msp430fr2100.h
include/msp430fr2110.h
include/msp430fr2111.h
include/msp430fr2153.h
include/msp430fr2155.h
include/msp430fr2310.h
include/msp430fr2311.h
include/msp430fr2353.h
include/msp430fr2355.h
include/msp430fr2422.h
include/msp430fr2475.h
include/msp430fr2476.h
include/msp430fr2512.h
include/msp430fr2522.h
include/msp430fr2672.h
include/msp430fr2673.h
include/msp430fr2675.h
include/msp430fr2676.h
include/msp430fr5041.h
include/msp430fr5043.h
include/msp430fr50431.h
include/msp430fr5720.h
include/msp430fr5721.h
include/msp430fr5722.h
include/msp430fr5723.h
include/msp430fr5724.h
include/msp430fr5725.h
include/msp430fr5726.h
include/msp430fr5727.h
include/msp430fr5728.h
include/msp430fr5729.h
include/msp430fr5730.h
include/msp430fr5731.h
include/msp430fr5732.h
include/msp430fr5733.h
include/msp430fr5734.h
include/msp430fr5735.h
include/msp430fr5736.h
include/msp430fr5737.h
include/msp430fr5738.h
include/msp430fr5739.h
include/msp430fr57xxgeneric.h
include/msp430fr5962.h
include/msp430fr5964.h
include/msp430fr5992.h
include/msp430fr5994.h
include/msp430fr59941.h
include/msp430fr6005.h
include/msp430fr6007.h
include/msp430fr6035.h
include/msp430fr6037.h
include/msp430fr60371.h
include/msp430fr6041.h
include/msp430fr6043.h
include/msp430fr60431.h
include/msp430fr6045.h
include/msp430fr6047.h
include/msp430fr60471.h
include/rf430frl152h.h
include/rf430frl152h_rom.h
include/rf430frl153h.h
include/rf430frl153h_rom.h
include/rf430frl154h.h
include/rf430frl154h_rom.h