Hi team,
The MCU operates at 3.3V, but only has a voltage waveform of about 1.8V, and the LCD is very attenued and requires a certain angle to see the residual image. The part that needs to be displayed as a number also shows the non-numeric exception. And when the power is disconnected and then restored, the LCD display goes off and the display returns to normal.
Issues:
1. Does the MSP430F449 have this kind of bug in the LCD driver module?
2. 2.Why does the total power supply disconnect and then power back up to return to normal? The power supply is a 3.6V battery, and it's all new, and it has both an LDO and tantalum capacitance and MLCC regulation and filtering on the circuit. The customer would like to know is there anything else could be wrong?
Could you help check this case? Thanks.
Best Regards,
Cherry