I am writing a program to calculate the mel-frequency coefficients of an audio signal using the spectrum - for the same, I want to use the support of an embedded RTOS - one of the references I have is written in RT Thread - while I looked at different questions on the forum and in general that mention free RTOS, TI-RTOS and so on. I would still like to confirm from someone from the TI Team as to whether RT Thread is supported on the MSP430FR5994. Also, please let me know if I need to re-direct this question to a different forum in case that would be more helpful.
Thanks!