Other Parts Discussed in Thread: MSP430F5529,
Hi Ti Experts,
Do we have any examples related to Sequence-of-Channels Mode? I'm trying to configure mine but I'm unable to get input in that.
//P1.5 - A5 - Pin 5 P1SEL0 |= BIT5; P1SEL1 |= BIT5; //P3.1 - A13 - Pin 3 P3SEL0 |= BIT1; P3SEL1 |= BIT1; // Configure ADC12 ADC12CTL0 = ADC12SHT0_2 | ADC12ON | ADC12MSC; //16 clock cycles sampling, ADC on, multiple sample. ADC12CTL1 = ADC12SHP | ADC12SSEL_3 | ADC12CONSEQ_1; //Pulse mode. ADCCLK = SMCLK. Sequence-of-Channels Mode autoscan. ADC12CTL2 = ADC12RES_2; //12-bit conversion results ADC12CTL3 = ADC12CSTARTADD_1; // Configure ADC input channels ADC12MCTL1 = ADC12INCH_5 | ADC12VRSEL_0; //A2 ADC input select; Vref=VCC=3.3V ADC12MCTL2 = ADC12INCH_13 | ADC12VRSEL_0 | ADC12EOS; //A3 ADC input select; Vref=VCC; End-of-sequence ADC12CTL0 |= ADC12ENC | ADC12SC; Here is my ADC ISR code: #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = ADC12_B_VECTOR __interrupt void ADC12_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(ADC12_B_VECTOR))) ADC12_ISR (void) #else #error Compiler not supported! #endif { switch (__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG)) { case ADC12IV__NONE: break; // Vector 0: No interrupt case ADC12IV__ADC12OVIFG: break; // Vector 2: ADC12MEMx Overflow case ADC12IV__ADC12TOVIFG: break; // Vector 4: Conversion time overflow case ADC12IV__ADC12HIIFG: break; // Vector 6: ADC12BHI case ADC12IV__ADC12LOIFG: break; // Vector 8: ADC12BLO case ADC12IV__ADC12INIFG: break; // Vector 10: ADC12BIN case ADC12IV__ADC12IFG0: break; // Vector 12: ADC12MEM0 case ADC12IV__ADC12IFG1: var1 = ADC12MEM0; break; // Vector 14: ADC12MEM1 case ADC12IV__ADC12IFG2: var2 = ADC12MEM1; break; // Vector 16: ADC12MEM2 case ADC12IV__ADC12IFG3: break; // Vector 18: ADC12MEM3 case ADC12IV__ADC12IFG4: break; // Vector 20: ADC12MEM4 case ADC12IV__ADC12IFG5: break; // Vector 22: ADC12MEM5 case ADC12IV__ADC12IFG6: break; // Vector 24: ADC12MEM6 case ADC12IV__ADC12IFG7: break; // Vector 26: ADC12MEM7 case ADC12IV__ADC12IFG8: break; // Vector 28: ADC12MEM8 case ADC12IV__ADC12IFG9: break; // Vector 30: ADC12MEM9 case ADC12IV__ADC12IFG10: break; // Vector 32: ADC12MEM10 case ADC12IV__ADC12IFG11: break; // Vector 34: ADC12MEM11 case ADC12IV__ADC12IFG12: break; // Vector 36: ADC12MEM12 case ADC12IV__ADC12IFG13: break; // Vector 38: ADC12MEM13 case ADC12IV__ADC12IFG14: break; // Vector 40: ADC12MEM14 case ADC12IV__ADC12IFG15: break; // Vector 42: ADC12MEM15 case ADC12IV__ADC12IFG16: break; // Vector 44: ADC12MEM16 case ADC12IV__ADC12IFG17: break; // Vector 46: ADC12MEM17 case ADC12IV__ADC12IFG18: break; // Vector 48: ADC12MEM18 case ADC12IV__ADC12IFG19: break; // Vector 50: ADC12MEM19 case ADC12IV__ADC12IFG20: break; // Vector 52: ADC12MEM20 case ADC12IV__ADC12IFG21: break; // Vector 54: ADC12MEM21 case ADC12IV__ADC12IFG22: break; // Vector 56: ADC12MEM22 case ADC12IV__ADC12IFG23: break; // Vector 58: ADC12MEM23 case ADC12IV__ADC12IFG24: break; // Vector 60: ADC12MEM24 case ADC12IV__ADC12IFG25: break; // Vector 62: ADC12MEM25 case ADC12IV__ADC12IFG26: break; // Vector 64: ADC12MEM26 case ADC12IV__ADC12IFG27: break; // Vector 66: ADC12MEM27 case ADC12IV__ADC12IFG28: break; // Vector 68: ADC12MEM28 case ADC12IV__ADC12IFG29: break; // Vector 70: ADC12MEM29 case ADC12IV__ADC12IFG30: break; // Vector 72: ADC12MEM30 case ADC12IV__ADC12IFG31: break; // Vector 74: ADC12MEM31 case ADC12IV__ADC12RDYIFG: break; // Vector 76: ADC12RDY default: break; }
I cannot see any of the ADC12MEMx register values are getting updated. Can anyone point it out what am I doing wrong? Is there any wrong in configuration or something else?
Please reply as soon as possible I shall be grateful for that as I have tried alot and I have not found any inputs on the ADC12MEMx registers. Even there are no examples
given by Ti
so I'm struggling to figure it out what am I doing wrong?