This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6047: How to change the USS parameter UPS0 to UPS1 Gap (ms) via UART during runtime without using USSD Center.

Part Number: MSP430FR6047

Hi Everyone,

I am trying to change the UPS0 to UPS1 Gap (ms) during runtime via UART, I am using the example code FR6047_USSSWLib_template_example. In certain scenario I want to bring the gap USS_SYS_MEASUREMENT_PERIOD to 1638(50ms) from 32768(1000ms) via  UART from another module. I am using a CUSTOM PCB in which my MSP430FR6047 can communicate with another device via UART. Please direct me to the best way to achieve this. 

Thanks in advance.

**Attention** This is a public forum