Other Parts Discussed in Thread: TM4C123FH6PM
there is no ready-made soluion.
So my task is: I have a legacy board in all of devices, it's based on MSP430F2418 and it is a production board, so it cannot be altered.
I have a small communication board, connecting all the stack devices with CAN bus, and this board have a connection to target boiard's JTAG interface. BSL pins are occupied on the target device, so we cannot use them.
Using the code from a topic I mentioned above I can erace the FLASH on the target board, but when I am writing the FLASH contents it is appearing to be corrupt.
Is there any suitable documentation nor sample code on using Tiva MCU for flashing MSP430? Or any other option?
This task is very critycal for us.
Thank you!