Other Parts Discussed in Thread: ENERGIA, MSP430FR2355, MSP-EXP430G2ET,
I'm receiving the following error in Energia when trying to upload any code. I have the correct board chosen in Energia and the correct COM. I've confirmed that
#elif defined (__MSP430FR2355__)
#include "msp430fr2355.h"
is included in the msp430.h file. My MSP-EXP430G2ET works in Energia but not the MSP-EXP430FR2355. It works perfectly fine in CCS just not Energia. This happens no matter the code. Thank you in advance to any help.
- In file included from C:\Users\XXX\AppData\Local\Energia15\packages\energia\hardware\msp430\1.0.7\cores\msp430/Energia.h:4:0,
- from C:\Users\XXX\AppData\Local\Energia15\packages\energia\hardware\msp430\1.0.7\cores\msp430/Arduino.h:3,
- from sketch\sketch_nov14a.ino.cpp:1:
- c:\users\XXX\appdata\local\energia15\packages\energia\tools\msp430-gcc\4.6.6\bin\../lib/gcc/msp430/4.6.3/../../../../msp430/include/msp430.h:1793:2: error: #error "Failed to match a default include file"
- exit status 1
Error compiling for board MSP-EXP430FR2355LP.