Hi,
I am using Sigma Delta ADC in MSP430F6736A to convert an Input signal of 13.5Hz with 100mVpp amplitude and 50mV offset.
SMCLK is used as SD24_B clock source and OSR =607
But output has more than 24 bits . And when I am converting it to voltage using
voltage[i]=(float)(results[i]*3/con); //con=0x1000000(2^24)
Voltage[i] is around 20 but the input signal is 100mVpp with 50mV offset. When Voltage is calculated after removing offset from results[i] result voltage is between -200.36mV and 200.756mV
Please help me with suggestions on what could be going on here.
Thanks & regards,
Anusree