Setup:
Communication with the design center via IC bulk transfer via Captivate ISO adapter to Captivate PGMR.
The channel bar of the electrode is displayed, so the deflection that there is a touch.
However, the interface always starts with the Conversion Count 500, so I assume that is the default value.
This cannot be adjusted. I first thought I found the error yesterday because there was a cold solder joint on the pull-up of the IRQ pin.
After I went to test again today, the same problem occurred.
Do you have any idea where this error could come from?
Translated with www.DeepL.com/Translator (free version)