Good morning,
I have a problem in configuring the internal reference Vref = 1.2 V of the ADC SD16_A as an output in the microcontroller MSP430F2013. Indeed, following the datasheet, I set the bits SD16VMIDON = 1 and SD16REFON = 1 of the register SD16CTL but when I measure the voltage at pin P1.3 (the one associated with the Vref) I don't see the 1.2 V. The pin is floating but I have also tried to insert a bypass capacitor as suggested in the datasheet and nothing changed.
Am I doing anything wrong or missing anything?
Thank you,
Alessandro