I just got this board and have been going trough the code examples in the collateral files. All are working with the exception of the Voice Recorder. I've had to make minor changes in some cases. (Does LCDMEM[0] really refer to LCDMEM1 ? That's weird.)
CCS4 doesn't accept the following:
__root unsigned int DMA2CTL_Const_R = DMADSTINCR_3 + DMAEN + DMAIE;
The error is:
a value of type "unsigned int" cannot be assigned to an entity of type "__SFR_FARPTR"
This code tries to set up the DMA to address the second 64k of flash.
I will post this on the CCS4 forum as well.
Andy