Other Parts Discussed in Thread: MSP-FLASHER
Hi Experts,
Our customer is having a problem flashing the device MSP430FR2475 using EXP430FR2355 board via the JTAG pins TDIO/TCK using the MSPflasher tool.
Here is the full error message:
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...
- The entered filename is invalid.
-
- Please reenter the filename or enter n to abort: v2-flash.sh
* Checking for available FET debuggers:
* Found USB FET @ ttyACM0 <- Selected
* Initializing interface @ ttyACM0...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...done
* Accessing device...
# Exit: 16
# ERROR: Unknown device
* Starting target code execution...done
* Disconnecting from device...done
*
* ---------------------------------------------------------------------
Can you help with this?
Thank you.
Regards,
Marvin A.