Hi experts,
I´ve been working on a flow meter application, but I´m having some troubles with de Flow Rate calculation (non calibrated).
I´m working on mili-liters per second. The issue is that, when working on flow rates below 500 ml/s, it works all fine. But when I increase the reference flow up to 600 ml/s, I get some alteration in the flow, going from a real and reasonable measurement to an abnormal flow rate, as seen in the picture.
I´m using the following configurations. I'm using only, for now, the non calibrated value.8666.USS_meterVFRCalibFlowTemperature.h 2480.USS_intrplCorrLUT.h 6114.USS_temperatureLUT.h
I would really appreciate your help.
The picture shows the common values around 650 ml/s, but we get some values up to 3000 ml/s. We have also notice, using the USS GUI, that this values show when UPS increment its value, but DNS keeps a normal value.