Other Parts Discussed in Thread: MSP-GANG
Hi Team,
Can you have a look at the following customer software questions regarding MSP-Gang?
Programming via JTAG works, for remote control of the MSP-Gang I have 2 questions however :
1) Description in the manual unclear (SLAU358Q-September 2011-Revised October 2019).
3.5.3.1 Select Image Command
Tx -> 3E 50 4 4 A1 0 0 CKL CKH
Rx -> 90 (ACK)
The Select Image command sets a number for the current image. After this command, all operations that
the MSP-GANG performs use this image. The MSP-GANG supports 96 images, 0 through 15. The default
image after power on is 0.
A1: holds a number of the image to set (0x00 to 0x0F).
According to documentation section 2.1.9 the number of images was increased from FW 1.2.1.0. From 16 x 512KB to 96 x 64KB. The above description ..96 images, 0 through 15 is at least misleading.
With the normal remote control it seems to have remained with the 16 images, at least I can only reach the images at the block borders 1.0, 2.0, etc. with the call 3E 50 04 04 A1 00 00 00 CKL CKH
Subimages can apparently only be accessed via the MSP-GANG.dll (4.2.26 MSPGANG_SelectImage).
Is this correct?
2) Question about the MSP-GANG GUI interface
As far as I understand and have seen so far, the image is used to define the overall setup of the programming (FW, Target, PWS, JTAG-Speed, Fuse, ..) and for the programming only the image is called and the command for programming is issued.
I have created 4 images, 2 different FW versions on either Target 1 and 2. If I call the images with the MSP-GUI, the display of the target changes on the display of the MSP-Gang for example also immediately, seems thus OK.
The MSP-GUI surface shows however NO change.
Question about this:
How can I check the settings for an image afterwards?
I mean when I save an image on the HD and then load it again:
Which settings does the image contain?
Thank you,
Franz