Other Parts Discussed in Thread: MSP-EXP430FR2433, MSP430FR5869
Hello,
I am adding the interrupt functionality from a working UART TX example.
I tried putting a break at the switch case in the interrupt routine but it never triggers.
The code is mostly the same with the example here: dev.ti.com/.../node
Can anyone give me an advice?
Here is the code.
int main(void) { WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer P1DIR = 0x01; P1OUT = 0x00; P1REN = 0x00; P2DIR &= ~BIT3; // Set P2.3 as in P2REN |= BIT3; // enable pull-up/down resistor P2OUT |= BIT3; // pull-up resistor P2IES |= BIT3; // enable interrupt P1SEL1 &= ~(BIT4 | BIT5); // USCI_A0 UART operation P1SEL0 |= BIT4 | BIT5; UCA0CTLW0 |= UCSWRST; // Put USCI_A0 to software reset UCA0CTLW0 |= UCSSEL__SMCLK; // Use SMCLK(1048576Hz) for baud rate calculation UCA0BRW = 9; // N = f/BR = 1048576/115200 = 9 UCA0MCTLW = 8; UCA0CTLW0 &= ~UCSWRST; // Release USCI_A0 software reset UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt __bis_SR_register(GIE); //__bis_SR_register(LPM3_bits|GIE); //LPM3 not work when using SMCLK PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode to activate previously configured port settings while(1); } #pragma vector=USCI_A0_VECTOR __interrupt void USCI_A0_ISR(void) { switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG)) { case USCI_NONE: break; case USCI_UART_UCRXIFG: P1OUT ^= 0x01; UCA0TXBUF = UCA0RXBUF; break; case USCI_UART_UCTXIFG: break; case USCI_UART_UCSTTIFG: break; case USCI_UART_UCTXCPTIFG: break; default: break; } }