Hi team,
Here's two issues from the customer may need your help:
1. The BSL listed in the slau550aa documentation cannot be found in the MSP430BSL_1_02_00_01.zip file. As shown below.
2. The FRAM space of FR6043 is: 6000~15FFF, of which F000- OXFFFF is defined as bootloader.
When using the MSP430FRBoot_1_03_00_00 host routine to upgrade, the APP.TXT cannot be loaded, and the size is about 45K. But there is no problem with the smaller program.
Is it because after the bootloader is divided, the addresses before and after can not meet the 40K continuous address, which causes it to fail to load.
Thanks.
Best Regards,
Yale