This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-FR6043: "No connected HID devices" Ultrasonic Sensing Design Center (Water Mode)

Part Number: EVM430-FR6043
Other Parts Discussed in Thread: MSP430F5528, UNIFLASH

Hello,

I'm working on the "Optimized Ultrasonic Sensing Metrology Water Flow Measurement Reference Design" project on EVM430-FR6043. I built and ran the code on the board, but when I launch the  Ultrasonic Sensing Design Center Interface and try to connect it, I get the error: "No connected HID devices".

In principal, I configured jumpers correctly for Design Center communication (J1: 1-2 ON, 3-4: ON, 5-6: ON, 7-8: OFF and 9-10: OFF). Also, I configured jumpers so the board is powered by USB. The rest of jumpers haven't been touched since I bought the kit.

Thanks in advance,

Alberto

**Attention** This is a public forum