Other Parts Discussed in Thread: MSP430FR2433, MSP-FET
Hardware: MSP-EXP430FR2433, connect all jumpers from mainboard to FET board
Software: BSL scripter 3.4.0.1
Procedure
-Connect the board to the PC using a USB cable
-Download firmware using CSS. In this firmware, I inserted the instruction to jump to BSL
__disable_interrupt(); // disable interrupts ((void ( * )())0x1000)(); // jump to BSL
-Within 10s from powering the board, I started BSL scripter to download the firmware but it failed. I set the correct MSP Application COM port in the script file
The error was shown in the picture below. I searched all the related problems in the forum but could not find the solution. Please help/
//
//Script example FRxx UART BSL
//
//Device : MSP430FR6989
//Comm Bridge: MSP-BSL Rocket
//
//Download blink application through
//UART BSL in FRAM device
//
LOG
MODE FRxx UART 9600 COM9
//gives wrong password to do mass erase
RX_PASSWORD pass32_wrong.txt
//
//add delay after giving wrong password
//because the device does not give
//any response after wrong password applied
//
DELAY 2000
RX_PASSWORD pass32_default.txt
MASS_ERASE
//RX_DATA_BLOCK blinkLED_FR6989.txt
RX_DATA_BLOCK test.txt
//CRC_CHECK 0x4400 0x0020
SET_PC 0xC400
@c400
21 83 B2 40 80 5A CC 01 92 C3 30 01 D2 D3 04 02
D2 E3 02 02 B1 40 10 27 00 00 91 83 00 00 81 93
00 00 F6 27 FA 3F 03 43 31 40 00 30 B0 13 4A C4
0C 43 B0 13 00 C4 1C 43 B0 13 44 C4 32 D0 10 00
FD 3F 03 43 03 43 FF 3F 03 43 1C 43 10 01
@ff80
FF FF FF FF FF FF FF FF
@ffda
3C C4 3C C4 3C C4 3C C4 3C C4 3C C4 3C C4 3C C4
3C C4 3C C4 3C C4 3C C4 3C C4 3C C4 3C C4 3C C4
3C C4 3C C4 28 C4
q