MSP430F6747A wants to use the internal SD24B function, set the internal reference voltage to 2.5 to -2.5V, how to set; For example, if the value is 2.2V, what should I do
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430F6747A wants to use the internal SD24B function, set the internal reference voltage to 2.5 to -2.5V, how to set; For example, if the value is 2.2V, what should I do
Hi Songhao
I checked the description on page 767 of MSP430x5xx and MSP430x6xx Family User's Guide (Rev. Q)
The internal SD24_B reference provides one fixed voltage of approximately 1.2 V
Do you know which MCU system of MSP430 and whether the internal reference voltage of SD24_B can be set?
**Attention** This is a public forum