Good morning!
I have purchased an EVM430-FR6043 to use for flow rate and oxygen concentration measurement along with two 200kHz Jiakang transducers. While the provided GUI is good for flow rate, I would like to be able to read the TOF readings from the transducers in real-time to be able to do further calculations for oxygen concentration. I was wondering if anyone has done a project like this before, either reading from the board separately to the provided softwares or adjusting the GUI to add in oxygen concentration readings?
Thank you in advance