Other Parts Discussed in Thread: MSP-TS430RGZ48B
Hi experts,
Have there been any cases in the past where an oscillation error has occurred due to a bad communication path pattern (layout) when using the UART pins (P3.3/P3.4, P4.4/4.5)? Please tell us as much as you know.
Currently, we have a customer's board using MSP430F341, but there is a problem with the crystal oscillator suddenly stopping.
[Details]
- The occurrence rate is 1/500 units.
- The problem does not occur when only the clock is operated. The above test was performed using "MSP430F534x_uscia0_uart_03.c". No problem was observed when only internal oscillator or only external oscillator.
- Swapped the MSP430 on the problematic board(A) with the MSP430 on the non-problematic board(B), resulting in a problem on the A side and no problem on the B side.
- As a result of using the target board(MSP-TS430RGZ48B), a problem occurs on the A side and no problem occurs on the B side. Oscillation abnormality occurs when the UART line (Tx,Rx) is cross-talked. On the B side, no oscillation error occurs under the same conditions.
The above indicates that there is a possibility that the problem is caused by the external environment, but there is also a problem inside the MSP430. If there are any similar cases or possible factors other than the UART layout, we would appreciate it if you could let us know.
Best regards,
O.H