Hi,
My customer is adjusting the RX/TX resolution of the touchpad with the CapTIvate Design Center GUI. I have two questions about this.
Q1) "Desired Resolution X Axis" and "Desired Resolution Y Axis" are described as "The desired resolution may be set from 2 to 65535" in the explanation on the right of the GUI, but they can only be set up to 65534. Is the GUI working correctly?
Q2) They assume a resolution of 0-127, so when they set these values to 128, they now return values in the range 0-125.
Perhaps the range is corrected so that the ones place is 0 or 5. (Because setting the resolution to 9 returns a value of 0-5)
Is it possible to achieve a resolution of 0-127?
Their evaluation environment
- GUI version : 1_83_00_08
- Setting value other than the corresponding parameter
- Prameters of tuning tab
- Thouch Threshold: 20(Set All)
- Rejection Threshold: 30
- Upper trim X(Y) Axis: Same value as Desired Resolution X(Y) Axis
- Pin setting
- 6x6 pad pattern
- Prameters of tuning tab
Best regards,
Sasaki