Hi TI,
I am trying to use Ultrasonic transducer having pulse frequency 58KHz with EVM430FR6047, The default configuration in USS_Config/USS_userConfig.h is #define USS_F1_FREQ 1000000, with this default settings program runs and goes into while loop given in main.c. But As i update this #define USS_F1_FREQ 58000, this configuration fails and program does not go into while loop to read the sensor values.
So My question is Does this board support 58Khz transducer? If Yes then How to configure it correctly If I want to use.