Part Number: MSP-EXP430FR5739
Other Parts Discussed in Thread: ENERGYTRACE,
Hi,
I have been writing code for a new product using the part above. Functionally, the device is fine, but my code, which spends almost all of its time in a LPM4, is causing current draw of 2.4mA. This far too high, and can't be right. I've tried many example projects and they all take a large current like this.
I have also been unable to use EnergyTrace due to an error message "error communicating with FET USB1". All of the jumpers on the board are present, but the current doesn't change much whether they are there or not.
Do you have any "expected" currents for the particular example projects available for this board (so that I can test them) or could you test them for me please?
I am using a Keysight 34450A on 100mA range across the VCC jumper.
Can you tell me why the EnergyTrace doesn't work for me.. I've tried changing settings but nothing seems to work?
thank you
David