This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSP430FR2476: Voltage drop on input with an external pull up

Part Number: LP-MSP430FR2476
Other Parts Discussed in Thread: MSP430FR2475

Hello, 

I am designing a product with a MSP430FR2475 microcontroller but in order to  become familiar with the uc, I am using a LP-MSP430FR2476 .

I need to get the state of 12 IO in my project, so,as a test, I added an external pull up resistor on one input to see how the micro behaves. Seing that my system has to consumme as less as possible, I put a 1Mohm resistor as pull up, so it doesn't consumme too much when the I/O is putted to the ground.

But with a 1Mohm pull up resistor and powering the board by USB, I have a drop of voltage of 1.7V. Even with a 100kohm resistor my voltage dropped about 300mV. 

Wanting to power up my microcontroller with some 2.2V I can't afford some big drops like those on my inputs. 

 

I would like to know if you have any advise on how to reduce those drops, may be a soft features or anything.

 

Best regards, 

Thibaud HABRAND, AXEM Technology

  1Mohm resistor.

  100kohm resistor.

**Attention** This is a public forum