I have an MSP430F5506 with a single I/O pin shorted to ground. The short is in the part, not my board. It persists when the parts is removed and ohmed out unpowered. The part works apart from this pin being shorted.
On the board, this pin is connected only to a transistor (FDV303N) gate. The transistor's source and drain are connected to a load well within the transistor's parameters. The trace does not pass near other traces.
I can't imagine anything in software could damage the I/O driver. So something goin on on that pin is causing my problem.
Question: What bad things could be happening to an I/O pin that would cause it to fail shorted to ground? Does it sounds like ESD, overvoltage, excessive current sourcing, excessive sinking, etc?
Thanks for any help!