Part Number: TIDM-SINGLEPHASEMETER
I am using the TIDM-SINGLEPHASEMETER (slaa517f.pdf) reference design in the implementation of a utility grade meter for an EV charging application (Based on TIDA-00637) and I have a question about the implementation of the Analog Front End (AFE) that is shown on page 5 of slaa517f.pdf. We are trying to measure the power consumed on 240VAC lines, in conjunction with a switching mode power supply (SMPS) instead of the provided capacitive power supply (we have many other features that require significantly more power). The issue we have is that the V- connection needs to be connected to the -120VAC (L2) line through a voltage divider, for which a circuit is not provided in the reference design. Also, the V- signal can not be directly connected to the ground of the MSP430, which is connected to the low-side of the SMPS, which is tied to Earth ground, as that would be completely unsafe. We have prototyped the attached AFE, but have had some issues with the readings. The MSP430 SDC impedance is modeled as a resistance using the values provided in the datasheet (200k per channel, 400k between the channels). I just want to check this is the right approach.