Part Number: MSP430FR5994
Hello,
For the following RTC example below, how is the interrupt triggered every 1 second? If I did the math correctly, the output of RT1PS is 250 Hz: 34KHz/4 (RTCPS0CTL divides by 4) /16 (RTCPS1CTL divides by 16).
So at 250Hz, the period would be given as .004 seconds. How does the code make this toggle the LED every 1 second?
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR69xx Demo - RTC in Counter Mode toggles P1.0 every 1s
//
// This program demonstrates RTC in counter mode configured to source from ACLK
// to toggle P1.0 LED every 1s.
//
// MSP430FR6989
// -----------------
// /|\ | |
// | | XIN|--
// ---|RST | 32768Hz
// | XOUT|--
// | |
// | P1.0|-->LED
//
// William Goh
// Texas Instruments Inc.
// August 2014
// Built with IAR Embedded Workbench V5.60 & Code Composer Studio V6.0
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1OUT &= ~BIT0;
P1DIR |= BIT0;
PJSEL0 = BIT4 | BIT5; // Initialize LFXT pins
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure LFXT 32kHz crystal
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL4 &= ~LFXTOFF; // Enable LFXT
do
{
CSCTL5 &= ~LFXTOFFG; // Clear LFXT fault flag
SFRIFG1 &= ~OFIFG;
} while (SFRIFG1 & OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers
// Setup RTC Timer
RTCCTL0_H = RTCKEY_H; // Unlock RTC
RTCCTL0_L = RTCTEVIE; // RTC event interrupt enable
RTCCTL1 = RTCSSEL_2 | RTCTEV_0 | RTCHOLD; // Counter Mode, RTC1PS, 8-bit ovf
RTCPS0CTL = RT0PSDIV1; // ACLK, /8
RTCPS1CTL = RT1SSEL1 | RT1PSDIV0 | RT1PSDIV1; // out from RT0PS, /16
RTCCTL1 &= ~(RTCHOLD); // Start RTC
__bis_SR_register(LPM3_bits | GIE); // Enter LPM3 mode w/ interrupts enabled
__no_operation();
return 0;
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=RTC_VECTOR
__interrupt void RTC_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(RTCIV, RTCIV_RT1PSIFG))
{
case RTCIV_NONE: break; // No interrupts
case RTCIV_RTCOFIFG: break; // RTCOFIFG
case RTCIV_RTCRDYIFG: break; // RTCRDYIFG
case RTCIV_RTCTEVIFG: // RTCEVIFG
P1OUT ^= BIT0; // Toggle P1.0 LED
break;
case RTCIV_RTCAIFG: break; // RTCAIFG
case RTCIV_RT0PSIFG: break; // RT0PSIFG
case RTCIV_RT1PSIFG: break; // RT1PSIFG
default: break;
}
}