Part Number: MSP430FR5969
We have a very small amount of code to place in RAM on our chipset. Our old programmer used LabView to do this. We would like to just use CCS or command prompt via USB or MSPGang. We are looking for a programmer to assist. This is the file we are trying to write to RAM.
data path: C:\foo
power trip: 22
vswr trip: 15
gain table min,max: 15,40
fwd PDgain min,max: 75,150
rev PDgain min,max: 140,250
final settings: +data, aget, 32766 maxpwr!
firmware: 3.0.1
Thank you,
Michael