Hi,
Would like to check regarding to the crystal selection for the F4618. Has previously tried to use the 12.5pF and 7pF load cap crystal to match with the F4618 which has internally set to 10pF. However, the results seems to be little far off. There is no external capacitor used. Read the SLAA225, SLAA322 and SLAA423 on the crystal selection, understand that when selecting the higher load cap of crystal will yield better accuracy, however it does not seems to be the case.
Any advise on this? Thanks..