Hi, I've got very simple code which is sampling from the ADC module of a potentiometer on P8.1 A9 to control a servo motor PWM which in turn rotates the SG90 servo motor.
The following code works fine for P1.7 output for PWM signal and using timer TA0 module
// Main c file
/********************************
main.c
Default Template file for testing purposes
Aaron Shek, @ 2023 University of Strathclyde
*********************************/
#include <msp430.h>
#include <driverlib.h>
#include <stdio.h>
unsigned int rate_ = 0;
uint32_t TimerA0_period = 20000; // PWM Period
unsigned int i;
// ADC interrupt service routine
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_ADCIFG:
rate_ = (int)(600 + (2.05*ADCMEM0)); // Max value of 2695, min 600
//printf("%d\n",rate_);
__bic_SR_register_on_exit(LPM0_bits); // Clear CPUOFF bit from LMP0 to prevent MCU sleeping
//ADC_clearInterrupt(ADC_BASE,ADC_COMPLETED_INTERRUPT);
break;
}
}
void main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P1DIR |= 0x80; // P1.7 output
P1SEL0 |= 0x80; // P1.7 options select
P4DIR |= 0x01; // Indicator LED
P4OUT |= 0x01;
// Configure Pin for ADC
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P8,GPIO_PIN1,GPIO_PRIMARY_MODULE_FUNCTION);
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5; PMM_unlockLPM5();
// Timer TA0 setup
TA0CCR0 = TimerA0_period; // PWM Period
TA0CCTL1 = OUTMOD_7; // CCR1 reset/set
TA0CTL = TASSEL_2 | MC_1; // SMCLK, up mode
// ADC setup
// Configure the Pin
SYSCFG2 |= ADCPCTL9; // Turn on analogue pin A9 (so it is not a GPIO).
// Configure CLock source, operation mode
ADCCTL0 |= ADCSHT_2 | ADCON; // 16 ADCCLK cycles, turn on ADC.
ADCCTL1 |= ADCSHP; // ADDCLK = MODOSC; sampling timer
ADCCTL2 |= ADCRES; // 10 bit conversion results
// Configure ADC mux and +ve & -ve references
ADCMCTL0 |= ADCINCH_9; // A9 ADC input select; Vref = AVCC
ADCIFG &= ~0x01; //Clear interrupt flag
ADCIE |= ADCIE0; //Enable ADC conversion complete interrupt
__enable_interrupt();
while(1) {
ADCCTL0 |= 0x03; // Sampling and conversion start
while(ADCCTL0 & ADCBUSY) {
int memval = rate_;
TA0CCR1 = memval;
__delay_cycles(10000);
}
}
// __bis_SR_register(LPM0_bits); // Enter LPM0
}
However, when I want to use P8.3 instead alongside timer TA1 module instead using the exact same configuration it does not work:
// Main c file
/********************************
main.c
Default Template file for testing purposes
Aaron Shek, @ 2023 University of Strathclyde
*********************************/
#include <msp430.h>
#include <driverlib.h>
#include <stdio.h>
unsigned int rate_ = 0;
uint32_t TimerA1_period = 20000; // PWM Period
unsigned int i;
// ADC interrupt service routine
#pragma vector=ADC_VECTOR
__interrupt void ADC_ISR(void)
{
switch(__even_in_range(ADCIV,ADCIV_ADCIFG))
{
case ADCIV_ADCIFG:
rate_ = (int)(600 + (2.05*ADCMEM0)); // Max value of 2695, min 600
//printf("%d\n",rate_);
__bic_SR_register_on_exit(LPM0_bits); // Clear CPUOFF bit from LMP0 to prevent MCU sleeping
//ADC_clearInterrupt(ADC_BASE,ADC_COMPLETED_INTERRUPT);
break;
}
}
void main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
P8DIR |= 0x03; // P8.3 output
P8SEL0 |= 0x03; // P8.3 options select
P4DIR |= 0x01; // Indicator LED
P4OUT |= 0x01;
// Configure Pin for ADC
GPIO_setAsPeripheralModuleFunctionOutputPin(GPIO_PORT_P8,GPIO_PIN1,GPIO_PRIMARY_MODULE_FUNCTION);
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5; PMM_unlockLPM5();
// Timer TA0 setup
TA1CCR0 = TimerA1_period; // PWM Period
TA1CCTL1 = OUTMOD_7; // CCR1 reset/set
TA1CTL = TASSEL_2 | MC_1; // SMCLK, up mode
// ADC setup
// Configure the Pin
SYSCFG2 |= ADCPCTL9; // Turn on analogue pin A9 (so it is not a GPIO).
// Configure CLock source, operation mode
ADCCTL0 |= ADCSHT_2 | ADCON; // 16 ADCCLK cycles, turn on ADC.
ADCCTL1 |= ADCSHP; // ADDCLK = MODOSC; sampling timer
ADCCTL2 |= ADCRES; // 10 bit conversion results
// Configure ADC mux and +ve & -ve references
ADCMCTL0 |= ADCINCH_9; // A9 ADC input select; Vref = AVCC
ADCIFG &= ~0x01; //Clear interrupt flag
ADCIE |= ADCIE0; //Enable ADC conversion complete interrupt
__enable_interrupt();
while(1) {
ADCCTL0 |= 0x03; // Sampling and conversion start
while(ADCCTL0 & ADCBUSY) {
int memval = rate_;
TA1CCR1 = memval;
__delay_cycles(10000);
}
}
// __bis_SR_register(LPM0_bits); // Enter LPM0
}
I'm very lost and I've consulted the user guide and datasheet but I cannot see where I went wrong.

Your help is much appreciated.
Aaron