Part Number: TIDM-CAPTIVATE-THERMOSTAT-UI
Hi
My costomer have a question about CapTIvate reference designe.
In This document, 4.3.4 Electrode Geometry
--
Capacitive Touch Thermostat User Interface With CapTIvate TmTechnology
https://www.ti.com/lit/ug/tiduav1/tiduav1.pdf
--
"A ground plane is placed in the center of the sensor to keep the Rx and Tx electrode tightly coupled. The tight coupling that is forced between the two electrodes improves their resistance to external noise and allows for buttons which use this design to be spaced close together."
is witten.
Question1 : How to a ground plane effect RX and TX electrode tightly coupled.
I think fill RX pattern is good for big sensor capasitance between TX snd RX .
Question2 : The tight coupling (by a ground plane) is forced between the two electrodes improves their resistance to external noise. because TX-GND and RX-GND capacitance can be increased, So The level of noise in the sensing is relatively small compared to the voltage amplitude that the parasitic capacitance imparts to the sensing.
Is this correct?
Question3 : "Electrode tightly coupled" is improved by remove RX pattern section that can get capacitance less than another(Not removed) section?
Thanks,
GR