Other Parts Discussed in Thread: SYSCONFIG,
I'm using SDK 0.58 to configure two LP-MSPM0G3507 boards using the tx and rx example firmware. When in sysconfig, the "Desired Arbitration Rate (kbits/sec)" for the MCAN peripheral will not enable "1000" as an entry. It says "Must be in the range of 1 to 999"
1Mbps arbitration is supported in the CAN-FD spec and seems like it would be a popular value for high-bandwidth applications.
If it's just a sysconfig limitation, can you give me the settings needed in the entry boxes and I can turn off the autocalc feature. I'm using the 48MHz oscillator as the CAN clock.
Thanks!