Hi, I am testing with EVM430-FR6047 and my own design. I have two questions.
1. When I tested with EVM430-FR6047 board, I found out the value of C11,C12 have a relationship with time of receive Bias.
for the receive signal amplifier, If I change the C11,C12 to 2nF, is it no problem? and Can I get the value limit of capacitance? Min and Max
2. I hope to receive the TOF value and convert (double type) from FR6047, but I can't understand the "IQ40" fixed point.
Can I get the bit information of IQ40? following is what I understood but the result is not accurate.
Thanks for reply.