Part Number: MSP430F2370
Other Parts Discussed in Thread: TRF7960
Hi all,
I have an issue with a design around the MSP430F2370.
The software is running fine when the MCU is attached to MSP-FET430UIF, the uart communication is up and data can be exchanged.
This statement is true for both Debug and Release configuration.
However when the system is running in standalone mode (Debug or Release) the uart communication does not work anymore.
A led indicator on the board shows that the MCU speed is not the same with or without JTAG.
When signal SMCLK is observed, I see that its mean value is 6.85Mhz when the JTAG is connected, 3.39 MHz when the JTAG is not connected.
I can't figure out what is the problem.
Is there anyway to check the MCLK on this MCU ?
Do you have any advices to understand and solve this issue ?
Best regards