//******************************************************************************
// MSP430G2x21/G2x31 Demo - SPI full-Duplex 3-wire Master
//
// Description: SPI Master communicates full-duplex with SPI Slave using
// 3-wire mode. The level on P1.4 is TX'ed and RX'ed to P1.0.
// Master will pulse slave reset for synch start.
// ACLK = n/a, MCLK = SMCLK = Default DCO
//
// Slave Master
// MSP430G2x21/G2x31 MSP430G2x21/G2x31
// ----------------- -----------------
// | XIN|- /|\| XIN|-
// | | | | |
// | XOUT|- --|RST XOUT|-
// | | /|\ | |
// | RST/NMI|--+<----|P1.2 |
// LED <-|P1.0 | | P1.4|<-
// ->|P1.4 | | P1.0|-> LED
// | SDI/P1.7|<-------|P1.6/SDO |
// | SDO/P1.6|------->|P1.7/SDI |
// | SCLK/P1.5|<-------|P1.5/SCLK |
//
// D. Dang
// Texas Instruments Inc.
// October 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430g2221.h>
void main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer
P1OUT = 0x10; // P1.4 set, else reset
P1REN |= 0x10; // P1.4 pullup
P1DIR = 0x01; // P1.0 output, else input
USICTL0 |= USIPE7 + USIPE6 + USIPE5 + USIMST + USIOE; // Port, SPI master
USICTL1 |= USIIE; // Counter interrupt, flag remains set
USICKCTL = USIDIV_4 + USISSEL_2; // /16 SMCLK
USICTL0 &= ~USISWRST; // USI released for operation
USISRL = P1IN; // init-load data
P1DIR |= 0x04; // Reset Slave
P1DIR &= ~0x04;
for (i = 0xFFF; i > 0; i--); // Time for slave to ready
USICNT = 8; // init-load counter
_BIS_SR(LPM0_bits + GIE); // Enter LPM0 w/ interrupt
}
// USI interrupt service routine
#pragma vector=USI_VECTOR
__interrupt void universal_serial_interface(void)
{
if (0x10 & USISRL)
P1OUT |= 0x01;
else
P1OUT &= ~0x01;
USISRL = P1IN;
USICNT = 8; // re-load counter
}
hi all i found this example from net.. i don t know how should i check this example.. that is whether i should load this program to master as well as slave or else master alone.. then where should i give the input and how can i check whether the serial communication working or not..kindly help me any one am new to this controller??? thanks in advance