Hello:
We are using the extended flash memory of the MSP430F2416 device. Code Composer does not seem to generate the appropriate output for the extended flash memory range 0x10000-0x19000 (large memory model). I believe it only supports 16 bit addresses, because the high bit is clipped from these 17-bit addresses in the generated HEX file. In the past, we only used the MSP430F247 device which doesn't have this extra flash memory, so this issue never came up. Do you know how to generate a HEX file that supports this extended memory range?
Thanks again!
Paul