Are there two INDEPENDENT timers in the MSP430F2112, or is there one timer/counter and it is shared amongst two compare modules? In the data sheet it shows Timer0_A3...whatever that is supposed to mean, and there is a Timer1_A2. I am guessing that Timer0 works with three different modules: CCR0, CCR1, CCR2. Timer1 should work with two different modules: CCR0 and CCR1. I am having a problem differentiating between the two. For example: TACCTL0 is for Timer0_A3? TACCTL1 is for Timer1_A2? Do each of these have a separate interrupt?